AXIS#.ENDEFAULT
Description
AXIS#. ENDEFAULT sets the default state of the software enable on power up for axes not controlled by a fieldbus (AXIS#.CMDSOURCE other than 1). Set AXIS#.ENDEFAULT to 1, to enable an axis automatically on power-up. Set AXIS#.ENDEFAULT to 0, to have the axis disabled on power-up.
Example
Code
Queries the default state of Axis 2 on power-up:
--> AXIS2.ENDEFAULT 0
Automatically enables Axis 2 on power-up:
--> AXIS2.ENDEFAULT 1
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
N/A |
|
Range |
0 to 1 |
|
Default Value |
0 |
|
Data Type |
Integer |
| See Also | AXIS#.EN | AXIS#.CMDSOURCE |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported
Fieldbus Information
| Fieldbus |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
|---|---|---|---|---|---|---|---|---|
| EtherCAT |
AXIS1.ENDEFAULT | 0x5000 | 0xA | USINT | - | - | RW | False |
| AXIS2.ENDEFAULT | 0x5100 | 0xA | USINT | - | - | RW | False |
|
Copyright © 2018 Kollmorgen |
|